Reflective Memory Domain: Configuration

About this task

Typically, different devices write to one or more blocks of data on the reflective memory card. The CIMPLICITY station may have its area to write to, but mostly it reads the data other devices write.  

Each block of the reflective memory card is defined to be of a certain size and addressable by any one of the following.

  • Byte
  • Word (2 bytes)
  • Quad word (4 bytes) addressable.  

The CIMPLICITY Reflective Memory Devcom configuration tool does the following.

Procedure

  1. Provides the ability to define how the blocks of data will be used by the reflective memory devcom
  2. Creates a structure for the reflective memory.

    In configuration, each memory block is associated with a model.  The model may reflect a particular physical device or some other logical division defined by the user.  

    • Reflective Memory Domain: Open the Reflective Memory DEVCOM Configuration Tool
    • Reflective Memory Domain: Memory Layout