Square D SY/MAX Device Configuration

Procedure

  1. In the Device field, enter the name of the device you are configuring.
  2. In the Port field, select the Square D SY/MAX port to be used by the device.

    When you click OK to create the device, the Device Properties dialog box opens.