Square D SY/MAX Port Configuration

Procedure

  1. In the Protocol field, select SY/MAX from the list of available protocols.
  2. In the Port field, select the communication port that will be used for Square D communications.

    When you select OK to create the port, the Port Properties dialog box for the protocol opens.