Updating the Antenna Configuration Settings
About this task
There are two methods of getting the Allen-Bradley Intelligent Antenna communications enabler to update the antenna's configuration settings based on the modifications to the ABRFID.INI file.
- You can stop and restart the CIMPLICITY project. This is usually not a feasible thing to do.
- You can update the configuration settings dynamically for a particular antenna, without affecting the flow of data from the rest of the antennas in your project:
To updated the configuration settings dynamically, use the following procedure:
Procedure
- In the project's Configuration cabinet, select Dynamic from the Tools menu. You can now change the device properties without having to stop and restart the project.
- In the project's Configuration cabinet, double-click on the Devices icon. The Devices window opens and shows you a list of all of the devices (antennas) in your project.
- From the list of devices in the Devices window, double click on the antenna you wish to update. This opens the Device Properties dialog box.
- In the Device Properties dialog box for the antenna:
- Clear the Enabled check box.
- Click Apply.
- Check the Enabled check box.
- Click OK to close the dialog box.
- Close the Devices window.