amaru_add_update_ca
Call this subroutine to add alarm update information to the current IPC buffer with Change approval Information.
Syntax
Int amaru_add_update_ca (bodyptr, bodylen, first_seg,
alarm_id, fr_id, user_or_serv_id,
ref_id, action, seq_num, resp_type,
key, changeapproval_obj, ret_stat);
char *bodyptr;
int bodylen;
COR_BOOLEAN first_seg;
char alarm_id[LONG_NAME_LEN+1];
char fr_id[FR_ID_LEN+1];
char user_or_serv_id[COR_MAX(USER_ID_LEN, SERVICE_ID_LEN)+1];
char ref_id[AM_REF_ID_LEN+1];
AM_STATE_TYPE action;
int seq_num;
AM_RESP_TYPE resp_type;
AM_RESP_KEY key;
ChangeapprovalInfo *changeapproval_obj,
COR_STATUS *ret_stat;
Input Arguments
bodyptr
|
Pointer to the beginning of the message body of the IPC buffer. | |
bodylen
|
Maximum length of the message body. | |
first_seg
|
Boolean value specifying whether the current generation request should be the first request in the message. TRUE implies first segment. | |
alarm_id
|
Identifier of the alarm to be generated. | |
fr_id
|
Identifier of the factory resource for which the alarm is being generated. | |
user_or_serv_id
|
Used for labeling logged alarms. Usually this is the service_id of the sending process. The AMAP sends the user_id of the connected terminal.
|
|
ref_id
|
Used to specify unique alarms when multiple alarm definitions are generated for the same Factory Resources. Alarm uniqueness is defined by the combination of alarm_id , fr_id , and ref_id .
|
|
Note: The ref_id is not displayed directly on the Alarm Manager User Interface. The ref_id , when used, can be duplicated in a message field for display.
|
||
action
|
Specifies the update action to take. | |
seq_num
|
Only used by AMAP. Application programs should pass 0. | |
resp_type
|
Used to select the type of response desired from the AMRP. The application program has three choices: | |
AM_CAPTURED_RESP - AMRP
|
Responds once the message has been captured (sent to a slave process or journalled). | |
AM_FULL_RESP - AMRP
|
Responds once the message has been fully processed. A status segment is returned for each request in the original message. | |
AM_NO_RESP
|
No response from AMRP to indicate that an alarm message has been received. | |
Note: Only the resp_type in the first generation message of each segment is used. Therefore, it is not possible to intermix the type of responses desired within a single IPC message..
|
||
key
|
The key is useful when the resp_type is set to AM_FULL_RESP . The key allows the application program to match the status segments returned with the alarm generation/update requests. The key is specified by the application program and is returned as is by the AMRP.
|
|
changeapproval_obj
|
A pointer to the change approval information for the alarm update operation. |
Output Arguments
ret_stat
|
Pointer to status structure. |
Return Value:
Either COR_SUCCESS
, or COR_FAILURE
. If the function returns anything other than COR_SUCCESS
, additional error information can be found in ret_stat
. Other than the changeapproval_obj parameter, this function should in all ways conform to the behavior of amaru_add_update()
.