cor_logstatus

Write error information to the CIMPLICITY status log.

Syntax

void cor_logstatus( const TCHAR *proc,
    COR_BOOLEAN severe,
    COR_STATUS *status )

Input Arguments

proc The name of the function where the error is detected.
severe Is situation severe error (FALSE, TRUE, FATAL)
status Pointer to the status block containing error info.

Output Arguments

None

Return Value

None

The value is sent to the status log, which is viewed through the Log Viewer application.