cor_stamp_get_components_utcHR

Convert a UTC timestamp into its various components.

Syntax

void cor_stamp_get_components_utcHR(stamp, yyyy, mm, dd, hh,
                              min, sec, tt100Nano )
COR_STAMP *stamp;
int *yyyy;
int *mm;
int *dd;
int *hh;
int *min;
int *sec;
int *tt100Nano;

Input Arguments

stamp A valid CIMPLICITY UTC timestamp.

Output Arguments

yyyy The year, in the range 1970..9999.
mm The month, in the range 1..12.
dd The day of the month.
hh The hour, specified as a 24-hour clock.
min Minutes past the hour, in the range 0..59
sec Seconds, in the range 0..59
tt100Nano Fractional seconds, specified in 100 Nano seconds.

Return Value

NONE