dcrp_notify_unsolicited_data

Notifies the Toolkit that unsolicited data has been received (must be called before unsolicited data between polls can be processed).

Syntax

void dcrp_notify_unsolicited_data(int *status)

Input Parameters

None

Output Parameters

status

Contains the function completion status. Valid values are:

TOOLKIT_SUCCESS Function completed successfully.
TOOLKIT_FAILURE Function not completed.

Return Value

None