dcrp_set_device_down
Sets device to a "DEVICE DOWN" status.
Syntax
int dcrp_set_device_down(char *device_id,
int *status)
Input Parameters
device_id
Contains the Device ID for the device whose status is to be set DOWN (UNAVAILABLE).
Output Parameters
status
Is the function completion status. Valid values are:
TOOLKIT_SUCCESS | Function completed successfully. |
TOOLKIT_FAILURE | Function not completed. |
Return Value
This subroutine returns one of the following:
TOOLKIT_SUCCESS | Function completed successfully. |
TOOLKIT_FAILURE | Function not completed successfully. |
Important:
DCRP_SET_DEVICE_DOWN
cannot be called until
USER_READ_DATA
or
USER_READ_DIAG_DATA
is called first.