dcrp_set_device_up

Sets device to a "DEVICE UP" status.

Syntax

int dcrp_set_device_up(char *device_id,
                       int *status)

Input Parameters

device_id

Contains the Device ID for the device whose status is to be set UP (AVAILABLE).

Output Parameters

status

Is the function completion status. Valid values are:

TOOLKIT_SUCCESS Function completed successfully.
TOOLKIT_FAILURE Function not completed.

Return Value

This subroutine returns one of the following:

TOOLKIT_SUCCESS Function completed successfully. 
TOOLKIT_FAILURE Function not completed successfully.