dcrp_user_alarm
Generates or clears an alarm.
Syntax
void dcrp_user_alarm (char *alarm_msg,
char *gen_or_clr,
char *device_id,
int *status)
Input Parameters
alarm_msg
Is the alarm message to be displayed.
gen_or_clear
Defines whether the alarm is to generated or cleared. Valid values are:
- TOOLKIT_GENERATE_ALARM
- TOOLKIT_CLEAR_ALARM
device_id
Identifies the CIMPLICITY software device for which the alarm will be generated or cleared.
Output Parameters
status
Is the function completion status. Valid values are:
TOOLKIT_SUCCESS | Function completed successfully. |
TOOLKIT_FAILURE | Function not completed. |