Determine if a Customized Number of Domains will be Supported
By default, the number of device domains that any device may have is defined by the constant TOOLKIT_MAX_DEVICE_DOMAINS
, which is defined in
%BSM_ROOT%\api\include\inc_path\toolkit.h
.
This default may be made larger or smaller based on the requirements of the interface.
No more than 16384 domains may be defined although practical limitations based on the size of the device communication interface itself may dictate a lower limit.