Field Definitions for Alarm Manager File
Note: Fields
segs_to_proc
through
process_jrnl_prio
define tuning parameters used to control AMRP processing. These parameters are reserved for GE Intelligent Platforms use. If you feel that they need adjusting on your system, please call CIMPLICITY Technical Support before making any changes.
Fields dg_input_prio through process_jrnl_prio define how AMRP activities are scheduled. Each type of activity is assigned an initial effective priority. Each time an item is not processed, its priority is increased by one. The priority range is from 1 to 20.
Records in this file contain the following fields:
- alarm_mgr_id
- alloc_segs_to_proc
- auto_pnum
- autoupd_tout
- count_
- count_type
- date_mask
- dg_input_prio
- dyn_am_cont_mask
- dyn_am_video_mask
- gen_auto_prio
- jrnl_max
- jrnl_max_act_limit
- jrnl_min
- jrnl_status
- jrnl_timer_period
- master_input_prio
- process_allocq_prio
- process_auto_prio
- process_jrnl_prio
- process_updq_
- segs_to_proc
- service_id
- upd_terms_prio
- ur_input_prio