low_index
Lowest valid index value for the port; specified in decimal.
Valid range is '0' to '999' and '-1'
Note: If the port being defined is a single port that does not end in a digit, both the Low and High values should be set to '-1' to indicate that no range is allowed for this port prefix.