PM_flags

Process Management startup and shutdown options for this process. Set the flag according to the following:

1 Cause Process Management to wait for a check-in message from this process when it is initializing. This value must always be used.
2 Cause Process Management to not generate an alarm when the process terminates
8 The Process Manager can reset the Process Down alarm that gets generated when this process terminates.

You can sum values to combine options. For example, if you want to have Process Management wait for a check-in message and reset the Process Down alarm, enter a "9" in this field.