Subroutine Guidelines
- Required subroutines.
- Optional subroutines.
- Subroutines that must be customized.
- Read and write request note.
Required Subroutines
You must design the following subroutines irrespective of the supported options:
user_device_info()
user_protocol_info()
Optional Subroutines
Below is a list of subroutines that are optional regardless of implemented functions. These functions may be called within the enabler, but the templates for these subroutines should suffice when no customization is required.
- user_init()
- user_on_demand_response()
- user_open_port()
- user_proc_event_1()
- user_proc_event_2()
- user_proc_event_3()
- user_proc_event_4()
- user_proc_event_5()
- user_proc_event_6()
- user_proc_event_7()
- user_proc_event_8()
- user_proc_event_9()
- user_proc_event_10()
- user_remove_point()
- user_term()
Subroutines That Must Be Customized
Below is a list of subroutines that must be customized based on the list of supported features:
For | Subroutine |
Custom addressing |
|
Model verification |
|
Domain definition |
|
Reading device data |
|
Writing device data |
|
Writing point quality data |
|
Receiving unsolicited data |
|
Device status |
|
Reading diagnostic data |
|
Host redundancy |
|
Read and Write Requests Note
Read and Write requests to devices are often grouped to improve efficiency. A grouped request fails if any point in the group is invalid. For this reason, it is strongly recommended that regardless of addressing-mode, you should use user_valid_point() to verify that data at the configured memory location is readable if read requests are supported.