user_init
Performs enabler-specific initialization tasks. It is called when the enabler starts, and its uses might include setting up shared memory regions, signal handlers and exit handlers.
You can find the template for this subroutine in:
usrtm_init.c
Syntax
void user_init(int *status)
Input Parameters
None
Output Parameters
status
Indicates whether the function successfully obtained all of the requested information. Valid values are:
TOOLKIT_SUCCESS | Function completed successfully. |
TOOLKIT_FAILURE | Function did not complete successfully. |
Return Value
None.