user_open_port
Opens the port for communications.
You can find the template for this subroutine in:
usrtm_opport.c
Syntax
void user_open_port(char *port_id,
int *baud_rate,
int *parity,
int *status)
Input Parameters
port_id
Is a pointer to a character string containing port used for communications.
The name provided is in upper-case characters and identifies the port name on the computer.
baud_rate
Is the pointer to the baud rate selected for the given port_id .
parity
Is the pointer to the parity selected for the given port_id .
Valid values for serial ports are:
- TOOLKIT_NO_PARITY
- TOOLKIT_EVEN_PARITY
- TOOLKIT_ODD_PARITY
Output Parameters
status
Indicates whether the function completed successfully. Valid values are:
TOOLKIT_SUCCESS | Function completed successfully. |
TOOLKIT_FAILURE | Function did not complete successfully. |
Return Value
None.