user_term
Performs enabler-specific termination tasks. This function is called following a request from CIMPLICITY software for the enabler to terminate. Its uses include cleaning up shared memory regions and disassociating from the device.
You can find the template for this subroutine in:
usrtm_term.c
Syntax
void user_term(int *status)
Input Parameters
None
Output Parameters
status
Indicates whether the function successfully completed. Valid values are:
TOOLKIT_SUCCESS | Function completed successfully. |
TOOLKIT_FAILURE | Function did not complete successfully. |
Return Value
None.