user_valid_diag_point

Determines the validity of a diagnostic point.

You can find the template for this subroutine in:

usrtm_valdiagpt.c

Syntax

void user_valid_diag_point(DEVICE_DATA*device_struct,
                           ADDR_DATA*address_struct,
                           int *valid_pt,
                           int *comm_status,
                           int *status)

Input Parameters

device_struct

Is a pointer to the structure defining device data. DEVICE_DATA is a typedef to a structure defined in < inc_path/toolkit.h > .

address_struct

Is a pointer to the address from which the data was read. ADDR_DATA is a typedef to a structure defined in < inc_path/toolkit.h > .

Output Parameters

valid_pt

Defines whether the point is valid. Valid values are:

TOOLKIT_SUCCESS The point is valid
TOOLKIT_FAILURE The point is not valid

valid_pt is not a Boolean value.

comm_status

Indicates whether a status of TOOLKIT_FAILURE occurred as a result of a communication failure. Valid values are:

TOOLKIT_SUCCESS Failure is not due to communications failure.
TOOLKIT_FAILURE Failure is due to communications failure.

status

Indicates whether the function read all the data. Valid values are:

TOOLKIT_SUCCESS Function completed successfully.
TOOLKIT_FAILURE Function did not complete successfully. Check comm_status to see if the failure was the result of a communication failure.

Return Value

None.