Important: You do not have the latest version of CIMPLICITY! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the CIMPLICITY product page. For more information on upgrades, contact your Proficyl sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Communications Enabler Overview
About this task
Communications Enabler Visual representation.
Custom Communication Enabler overview.
Communications Enabler Visual Representation
The following illustration shows you how a custom communication enabler is integrated into the standard CIMPLICITY software environment.
Custom Communication Enabler Overview
Procedure
Build Custom Communication Enablers
Determine the functions to be supported.
Determine the device models to be supported and the memory locations to be made accessible for each device-supported model.
Write specialized routines for each supported function.
Use the build procedures provided by the Device Communications Toolkit to compile the specialized routines and create an executable.
Create Configuration
Before you can run the executable, you must create configuration files that identify:
The name of the executable
The port(s) the enabler can use
The device model(s) the enabler will support
The memory locations the enabler will support for each supported model (optional)
Execute the Customized Communications Enabler
After you create the executable and configuration files and place them in the appropriate locations, you may configure the enabler in CIMPLICITY software and run it.