About Points
Point configuration can be divided in the following categories
- Device point only configuration.
- Virtual point only configuration.
- Device and virtual point configuration (Alarms, View, limits, enumeration, conversion).
- Point and alarm change approval.
- Point technical reference.
CIMPLICITY collects or calculates point data that it distributes to:
- CimView screens that are configured in CimEdit.
- Alarm Viewer screens.
- Alarm printers.
- Logging tables.
- Other CIMPLICITY software options
The Workbench provides the following icons to access Point configuration components in addition to the Point Properties dialog box.
Note: Click a Point icon to display related documentation.

The collection and distribution of point data is handled by the Point Management subsystem. Point Management's primary functions are to:
- Update the point database as point values change.
- Generate point alarms when limits are exceeded.
- Make point data available to CIMPLICITY software applications.
- Synthesize new point values by arithmetically combining other points.