CimEdit Global Specifications
Procedure
-
Click the CimEdit button
.
- Click Global Configuration.
Results
The Global Configuration dialog box opens.

Features that can be shared globally include the following.
1 | General features that can be shared globally. |
2 | Global script load list. |
3 | Before Context Menu/Before Editor Context Menu global events. |
4 | Compatibility. |
5 | Global button selections. |
6 | Undo stack size for a CimEdit screen (CimEdit Options dialog box). |
Important: If CIMPLICITY has just been upgraded from CIMPLICITY v8.2 or lower to CIMPLICITY v9.0 copy a configured CimView.cfg file (saved from the previous version) so it is in the following location.
..\<CIMPLICITY installation>\Data\CimView.cfg
If this file has not been copied into the the ..\Data directory, all of the global configuration settings will be the default settings, not settings that you might have configured in the earlier version.
If you do not have a configured CimView.cfg file, use the dialog boxes to enter and apply the settings that are appropriate for your CIMPLICITY v9.0 system.