Open the Point Control Panel through CimView
About this task
Note: Viewing the Point Control Panel through CimView is available if the role assigned to your user ID has authorization .
The Point Control Panel provides you with a forum in which you can easily review and change point values and status during runtime.
Procedure
Results
The Point Control Panel opens displaying the points that are configured for the CimView screen or the selected object.

Note: If there are no points associated with the selected object, a message informs you. The Point Control Panel does not open.