About Alarm Cast Alarm Administrator
The following topics contain an overview of the CIMPLICITY Alarm Cast Alarm Administrator and Alarm Cast Alarm server.
- The Alarm Cast Administrator and Alarm Cast Alarm Administrator must be on the same machine.
- Warning messages might open during configuration that Alarm Cast cannot connect to the project if the Alarm Cast Gateway is not running.
Note: The Alarm Cast Gateway runs when the project is running.
Alarm Cast Alarm Administrator: Key Features | |
Alarm Cast Alarm Administrator: How it Works. | |
Alarm Cast Alarm Administrator Pre-configuration. | |
Alarm Cast Alarm Administrator Components. | |
Alarm Cast Alarm Administrator Tools | |
Alarm Cast Alarm Administrator Glossary |