About Change Management
- About Change Management overview.
- Change Management topics.
- CIMPLICITY options not supported in Change Management.
About Change Management Overview
Beginning with CIMPLICITY 7.0, several versions of configuration and files that apply to a single CIMPLICITY projector computer level configuration can be stored and retrieved on a Change Management ??(PCM) server.
- More than one local server can hold copies of the same CIMPLICITY project and maintain the project's integrity through the PCM.
- Each local server can store versions of the computer-based files.

1 | Local Server 1 holds the following projects: C1, M2, P1. | |
2 | Local Server 2 holds the following projects: P1, M2, C2. | |
3 | Change Management Server holds several versions of the following: C1, M2, P1, C2. |
Change Management Topics
- Entities Overview in Change Management.
- Enable computer management.
- Enable project management.
- Change Management procedures.
- Change Management client.
- Change Management best practices.
- Change Management technical reference.
CIMPLICITY Options not Supported in Change Management
The following are not supported in Change Management.
- Microsoft Cluster.
- Tracker.
- Order Execution Management.