Alarm Cast Alarm Administrator Tools: Users
If Windows or Windows Trusted is selected for the Alarm Cast Alarm server security, a User Security Configuration folder is added to the Tools tree, if it was not already there.
Do the following.

A | Select User Security Configuration in the Alarm Cast Alarm Administrator window left-pane. |
B | Click New User on the Alarm Cast Alarm Administrator window toolbar. |
Result: Tabs for the User profile display in the Alarm Cast Administrator right-pane.
Alarm Cast Administrator Users: Details Tab
Select the Details tab; details options to register users are as follows.

Field | Description | ||
User | |||
User ID | Valid Windows user. | ||
Domain | Domain the user logs into. | ||
Password | (Required with Windows Security) Password assigned to the logged in Windows user. | ||
Confirm | (Required with Windows Security) Re-entered password | ||
Security | Security levels are as follows. | ||
SERVER ADMINISTRATION |
Full rights to all features.
Important: : The SERVER ADMINISTRATION security level is required to access (open) applications. For almost all instances, it is recommended that SERVER ADMINISTRATION be assigned to registered Alarm Cast users.
|
||
USER | Can access only the Alarm Cast Client to send a manual message. | ||
Notes | |||
Notes | (Optional) Additional details about or for the user. |