Alarm Cast Gateway for CIMPLICITY: Options
Before using Alarm Cast Gateway for CIMPLICITY, configure the various settings that control the interface to the gateway.
Click the Tools>Options on the Alarm Cast Gateway menu bar.
An Options dialog box opens; options are as follows.

Option | Description | |
Data Source |
Installation will default the Data Source to FPAMGWCIMPADMIN , pointing to the Gateway for CIMPLICITY administrator database.
|
|
Server Reload | Enables the user to select when they want a reload to server: with every change, or only when requested. | |
Reload with every change | Reload will occur when the Save button is clicked. | |
Reload only when requested | You will be informed that there are data changes the server needs to be notified about and have the option to either send the reload before closing or close the system without reloading the changes. |