cnc_download.exe
Purpose
Download one or more files from the PC to CNC memory. Each file may contain a single part program or a sequence of part programs.
Correct usage
C:\> cnc_download <nodenum> <pathnum> <filespec1> [<filespec2>] [<filespec3>]&ldots;
Usage defined
|
Node number (configured HSSB card). | ||
|
CNC path. Enter one of the following. | ||
Value | Path | ||
0 | None | ||
1 | First | ||
2 | Second | ||
3 | Third | ||
4 | Fourth | Series 30i/31i/32i only | |
5 | Fifth | Series 30i/31i/32i only | |
6 | Sixth | Series 30i/31i/32i only | |
7 | Seventh | Series 30i/31i/32i only | |
8 | Eighth | Series 30i/31i/32i only | |
9 | Ninth | Series 30i/31i/32i only | |
10 | Tenth | Series 30i/31i/32i only | |
If the CNC does not support multiple paths, enter 0. | |||
|
File specification. Each file specification indicates a single file containing part program(s) to download. This may be a fully qualified filename or a filename in the current directory. |
Example
The contents of each file is downloaded to CNC memory and displays success or failure status when it is complete:
C:\> cnc_download 0 0 c:\O0001.pp c:\O0002.pp c:\O0003.pp
Beginning download:
C:\O0001.pp: Success
C:\O0002.pp: File open failed
C:\O0003.pp: Success
C:\>
The O0001.pp and O0003.pp part program files have been downloaded and registered in CNC memory. The part program O0002.pp could not be opened and was not processed.
The following is a list of possible errors:
- File not found.
- Failed to open file for reading.
- File contains bad program.
- CNC write protect.
- CNC out of memory.