cnc_edownload_tool.exe
Purpose
Download CNC File data.
The command line utility cnc_edownload_tool.exe downloads CNC file data from files on the PC to CNC memory.
Correct usage
The following is the correct usage.
C:\> cnc_edownload_tool <data> <ipaddr> <portnum> <pathnum> <filespec.csv>
User defined
|
CNC file data. Enter one of the following. | ||
parm | Parameter Data | ||
tofs | Tool Offset Data | ||
zofs | Work Zero Offset Data | ||
cmv | Custom Macro Variable Data | ||
pec | Pitch Error Compensation | ||
kbit | Keep Relay Data | ||
|
IP address of the CNC. | ||
|
Port number of the CNC. | ||
|
CNC path. Enter one of the following. | ||
Value | Path | ||
0 | None | ||
1 | First | ||
2 | Second | ||
3 | Third | ||
4 | Fourth | Series 30i/31i/32i only | |
5 | Fifth | Series 30i/31i/32i only | |
6 | Sixth | Series 30i/31i/32i only | |
7 | Seventh | Series 30i/31i/32i only | |
8 | Eighth | Series 30i/31i/32i only | |
9 | Ninth | Series 30i/31i/32i only | |
10 | Tenth | Series 30i/31i/32i only | |
If the CNC does not support multiple paths, enter 0. | |||
|
File specification of file to receive the uploaded data. This may be a fully qualified filename or a filename in the current directory in comma separate variable (.csv) format. |
Example
The contents of the file parm1000.csv is downloaded to the CNC parameter data table <ipaddr>, <portnum> and <pathnum>:
C:\> cnc_edownload_tool parm 3.26.7.150 8172 0 parm1000.csv
Downloading parm for parmall.csv: Success
C:\>
The file download_tool_log.csv is either created or overwritten with any errors during the download.
Following is a list of possible errors.
- Could not determine CNC type.
- Could not link to DLL.
- Failure to get directory info.
- Bad directory info returned.