Marquee Manager Gateway: How it Works
Marquee Manager Gateway for CIMPLICITY is another product in the Marquee Manager Suite of products and may reside on your Marquee Manager Server or access a Marquee Manager Server over a LAN or WAN connection.
The Marquee Manager Gateway for CIMPLICITY provides a bridge between CIMPLICITY project alarms and your Marquee Manager Server. Various routing rules can be defined by selecting available Resources, Alarms, Classes and alarm message text that have been configured in your CIMPLICITY project. When one of these rules is met, message text can be dispatched to your Marquee Manager Server, including embedding alarm and point values within the message text.
There are four valid alarm states that may be configured for each Routing Rule:
Generate | The alarm becomes active by meeting the rules defined in the CIMPLICITY Point Properties dialog box> Alarm tab. |
Acknowledged | The alarm is Acknowledged by an operator with Alarm Viewer or the point is set up to Auto Ack in the Alarm Options of that point. |
Reset | The alarm is back within normal parameters or the point is set up to Auto Reset under the Alarm Options of that point. |
Delete | The alarm has met the rules under the Deletion Requirements in the Alarm Options. |