Marquee Manager Gateway Tools: Users
If Windows or Windows Trusted is selected for the server security, a Tools tree with a Users folder is added to the Marquee Manager Gateway window left-pane.
Do the following.

A | Select Users in the Marquee Manager Gateway window left-pane. |
B | Click New User on the Marquee Manager Gateway window toolbar. |
A Details Tab displays; options to register users are as follows.

Field | Description | ||
---|---|---|---|
User | |||
Username | Valid Windows user. | ||
Domain | Domain the user logs into. | ||
Password | (Required with Windows Security) Password assigned to the logged in Windows user. | ||
Confirm | (Required with Windows Security) Re-entered password | ||
Security | Security levels are as follows. | ||
ADMIN |
Full rights to all features.
Important: The ADMIN security level is required to access (open) applications. For almost all instances, it is recommended that ADMIN be assigned to registered Alarm Cast users.
|
||
DEFAULT | (Optional) Additional details about or for the user. | ||
Notes | |||
Notes | (Optional) Additional details about or for the user. |