SPC Charts: Attributes
SPC attribute charts provide different perspectives for reviewing defective units. What constitutes a defective unit depends on your definition (e.g. a unit might have to have three defects or certain type of defects to be classified as defective).
- Chart: nP
- Chart: P
- Chart: C
- Chart: U
- Chart: Exponentially Weighted Moving Average (EWMA)
- Chart: Report
Chart: nP
nP charts:
Track | Number of defective units in each sample. |
Report | Number of defective units in each sample. |
Note: Each unit is treated as pass or fail regardless of the number of defects it might have.
nP chart sample is:
- A constant:size.
- Normally collected in a frequency that emulates the process being evaluated.
- The nP chart is selected on the:
- Attribute Quality Characteristics Properties dialog box>General tab.
- SPC Control Properties dialog box>Chart tab.
- Control tests are available for the nP chart.
Chart: P
P charts:
Track | Number of defective units in each sample. |
Report | Proportion (percent) of defective units in each sample |
Note: Each unit is treated as pass or fail regardless of the number of defects it might have.
P chart subgroup is
- Possibly different from other subgroups in size.
- Normally collected in a frequency that emulates the process being evaluated.
- The nP chart is selected on the:
- Attribute Quality Characteristics Properties dialog box>General tab.
- SPC Control Properties dialog box>Chart tab.
- Control tests are available for the P chart.
Chart: C
C charts:
Track | Total number of defects in a unit. |
Report | Total number of defects in a unit. |
C chart subgroup is:
- Either:
- One item.
- A fixed number of items that are treated as one item.
- Assigned one or more defects to track.
- The C chart is selected on the:
- Attribute Quality Characteristics Properties dialog box>General tab.
- SPC Control Properties dialog box>Chart tab.
- Control tests are available for the C chart.
Chart: U
U charts:
Track | Total number of defects per unit that occur during the sampling period. |
Report | Mean (average) defects per unit during the sampling period. Note:Currently in CIMPLICITY SPC, the UCL is 1 or lower. |
U chart subgroup is:
- Able to have a different number of sampling units in each sampling period
- Assigned one or more defects to track.
- The U chart is selected on the:
- Attribute Quality Characteristics Properties dialog box>General tab.
- SPC Control Properties dialog box>Chart tab.
- Control tests are available for the U chart.
Chart: Exponentially Weighted Moving Average (EWMA)
EWMA charts
Track | Number of defective units in an observation. |
Report | Weighted subgroup mean, the more recent the sample, the higher the weight. Note: This detects much smaller process shifts than a normal control chart would |
EWMA observation is a rolling, fixed size weighted subset.
The EWMA chart is selected on the SPC Control Properties dialog box>Chart tab.
Chart: Report
Report charts display variable values in table format.
Optional fields that display on the Report chart are selected on the SPC Control Properties dialog box>Report tab.