Connection Error Handling
About this task
The PC must be able to communicate successfully with the CNC.
If communication fails, run the
test_cnc
utility in order to verify communication to the CNC.
Suggestions to resolve communication problems.
- HSSB.
- Ethernet.
HSSB
If you do not receive a response when you try to connect to the CNC.
Procedure
- Check to see if any other PC-vendor printed circuit board is using the HSSB assigned I/O address.
-
Check the rotary switch settings on the CNC-based HSSB printed circuit board.
The switch should be set to 1 to start up in normal mode. (If you change the setting, remember to cycle CNC power.)
- Reboot the PC and look at Windows Boot Log or the CIMPLICITY supportedoperating system System Log for errors that HSSB Driver is installed.
- Verify that the target CNC has the correct software and the option is enabled.
- Verify that the green LED located on the HSSB PC printed circuit board is ON after the CNC/ PC boot. This LED is visible from the rear of the PC next to the fiber optic connection.
-
Reboot the PC and CNC after changing any setup configuration data.
Ethernet
If you do not receive a response when you ping the IP address:
-
Check with your Network Administrator to ensure that the
- IP address is not in use by another device,
- Subnet mask is correct for the device.
- Reboot the PC and CNC after changing any setup configuration data.