Enable Project Management
Access Change Management Dialog Box
- Click Project>Properties on the Workbench menu bar, or click the Project Properties button on the Workbench toolbar. The Project Properties dialog box opens.
- Select the Change Management tab. Change Management options are as follows.
Enable Change Management
Do one of the following:
Check | Enables Change Management for the active CIMPLICITY project. |
Clear | Change Management is not enabled for the active CIMPLICITY project. This does not affect enabling Change Management for the computer project. |
- When Change Management is enabled for a CIMPLICITY project, the project’s Configuration Security on the Options tab is automatically checked and made read-only.
- Change Management can be enabled for both a running and a stopped project.
Configure Server
Name of Change Management server that the user will be using to authenticate/log in to Change management.
Test Connection
- Click Test connection to confirm that the selected Change Management server is available and can connect to the project. A Change Management Logon dialog box opens.
- Enter an authorized user name and password.
Results: One of the following will occur depending on the project/Change Management Server status.
- The connection is successful. A message opens and reports. The change management server connection test succeeded.
- The connection fails.
A message opens and reports: Unable to connect to change management server <Change Management server> with user <User Name>. Server unreachable or not found.
If the connection failed, check with the Change Management system administrator to correct the problem.
Requirement for logging into the Change Management server depends on the following.
Log on at Workbench startup/Prompt for user name and password at logon
If Change Management is enabled for the CIMPLICITY project, configuration security is enabled.
Other factors that determine if and when a user needs to log onto PCM include whether or not: the following are checked Yes or No:
- Allow Configuration Auto Logon in the Windows Authentication dialog box. If Allow Configuration Auto Logon is not checked, logging in options/requirements are the same as if the Windows Authentication login is invalid.
- Prompt Username/password.
- PCM Workbench Start.
If Allow Configuration Auto Logon is checked in the Windows Authentication window options and requirements for Change Management logon are as follows.
1 | Windows Logon for CIMPLICITY | Windows Logon for PCM |
Valid | Valid |
Windows Logon for CIMPLICITY | Windows Logon for PCM | ||
---|---|---|---|
VALID | VALID | ||
THEN | IF | TYPE | WHEN |
CIMPLICITY Logon | |||
Configuration Security | Yes | Auto | Workbench Start |
PCM Logon | |||
Prompt Username/Password | Yes / No | Manual / Auto | |
PCM Workbench Start | Yes / No | Workbench Start / PCM Open |
Windows Logon for CIMPLICITY | Windows Logon for PCM | ||
---|---|---|---|
VALID | INVALID | ||
IF | TYPE | WHEN | |
CIMPLICITY Logon | |||
Configuration Security | Yes | Auto | Workbench Start |
PCM Logon | |||
Prompt Username/Password | Yes / No | Manual / Manual | |
PCM Workbench Start | Yes / No | Workbench Start / PCM Open |
Windows Logon for CIMPLICITY | Windows Logon for PCM | ||
---|---|---|---|
Invalid | Valid | ||
IF | TYPE | WHEN | |
CIMPLICITY Logon | |||
Configuration Security | Yes | Manual | Workbench Start |
PCM Logon | |||
CIMPLICITY Login is Valid PCM Login | |||
Prompt Username/Password | Yes / No | Manual / Auto | |
PCM Workbench Start | Yes / No | Workbench Start / PCM Open | |
CIMPLICITY Login is Invalid PCM Login | |||
Prompt Username/Password | Yes / No | Manual / Manual | |
PCM Workbench Start | Yes / No | Workbench Start / PCM Open |
Windows Logon for CIMPLICITY | Windows Logon for PCM | ||
---|---|---|---|
Invalid | Invalid | ||
IF | TYPE | WHEN | |
CIMPLICITY Logon | |||
Configuration Security | Yes | Manual | Workbench Start |
PCM Logon | |||
CIMPLICITY Login is Valid PCM Login | |||
Prompt Username/Password | Yes / No | Manual / Auto | |
PCM Workbench Start | Yes / No | Workbench Start / PCM Open | |
CIMPLICITY Login is Invalid PCM Login | |||
Prompt Username/Password | Yes / No | Manual / Manual | |
PCM Workbench Start | Yes / No | Workbench Start / PCM Open |
Enter a Change Management Project Name
It is strongly recommended that this name be the same as the CIMPLICITY project name. The default name is the name of the local project. When the user first logs in, if the project does not exist in Change Management, the project is created. No files are added to the project except when specifically requested by the user.
Require Checkout Before Changes
Do one of the following.
Check | Require that an entity be checked out of Change Management before it can be edited. A message reminds a user that: You are required to check out the project before you can modify it.
|
Clear | An entity does not have to be checked out of Change Management to be edited and saved. |
Allow changes when the server is not available
Do one of the following.
Check | Allow changes when the Change Management server is not available. |
Clear | Do not allow changes when the Change Management server is not available. Important: If Require Checkout before changes is checked, configuration changes will not be possible if the Change Management Server is not available. |
Example:
- Allow changes when the server is not available is checked.
- A CimEdit screen, TANK750, is not checked out.
- TANK750 is enhanced with new graphic and text objects reporting additional point values.
- The following is done so these changes will be preserved.
- TANK750 is checked out. IMPORTANT: Don't overwrite local files with managed copy is checked.
- TANK750 is checked in.
Preserve runtime configuration data on fetch (passwords and alarm setups)
Prompt
The Preserve runtime configuration data on Fetch options dictate how the runtime data will be handled.
A Save Configuration Data dialog box opens with check box entries for each of the configuration data that has changed. The dialog box opens before any of the following processes are completed:
- Fetch.
- Check out.
- Get latest version.
Check the configuration data that you want to preserve:
- Passwords that were specified as valid after the checkout continue to be valid. A user who is logged in with a new password can continue configuration with no interruptions.
- New or modified alarm setups are preserved.
Click one more than one of the following:
- OK - Preserves or overwrites the configuration data based on your selection.
- Cancel - Cancels the retrieval.
- Select All - Checks all listed data check boxes. All listed data will be preserved.
- Clear All - Clears all the check boxes. All listed data will be overwritten.
Yes
- Passwords that were specified as valid after the checkout continue to be valid. A user who is logged in with a new password can continue configuration with no interruptions.
- New or modified alarm setups are preserved.
- When the base configuration is checked into Change Management, the file will be checked in with the current valid passwords.
No
- The file with the old passwords is fetched from Change Management and overwrites the file with the new passwords.
- The new passwords are no longer valid.
- A user will have to re-enter the old password and, in instances where a new password is required, the new password in order to continue configuration.
- When the base configuration is checked into Change Management, the file will be checked in with the passwords that were specified as valid after the checkout.
If the project has already been added to the Change Management server: a message opens and reports: Change Management project <project name> already exists on the Server <Change Management server>. Do you want to replace the project?
Click one of the following:
- Yes - Change Management maps your CIMPLICITY project to the existing Change Management project. The local project is now managed. The project (version) that was replaced is still on the Change Management server and can be retrieved, if necessary.
- No - The local project is Not added to the Change Management server. Not managed.
If the project is new on the Change Management server, the Change Management server maps a place for the Change Management project. The project is now managed.
Enable enhanced auditing
When the enhanced auditing check box is checked CIMPLICITY will put entries in the Change Management audit log when a point is added, modified or deleted.
- Point.
- Action.
- User who performed the action.