Marquee Manager Administrator Distribution Lists
About this task
Configured marquees can be added to distribution lists enabling the same message to be sent to multiple marquees with a single request.
Note: Marquee Manager Client applications provide the ability to compose messages and send them to a marquee distribution list, as to gateways.
Procedure
- Click the Distribution Lists folder in the Marquee Manager Administrator left-pane.
-
Click New Distribution List on the toolbar.
A Details tab displays; options are as follows.
Field Description Name Distribution List name. Description (Optional) Details to help identify the distribution list. Background Use either method to select the background color. - Choose a color from the dropdown list of predetermined colors,
- Click the color swatch to the right of the dropdown list; create a custom color.
Type Select which Type of Distribution List to create. Marquees that are listed in the Marquees box are determined by the Type. Available options include: - Bin Cell
- Solid Cell
- Stack Light
- Text Cell
- Text/Counter
- Tune
Marquees When a Type is selected, a list of configured marquees that are the selected type displays. Check the marquees that should be added to the distribution list. Tip: Check Show selected only to display only the marquees that will be included in the distribution list. - Click Save.
Results
Distribution list details are saved.