Marquee Manager Administrator Server
Procedure
-
Do the following.
- Expand Computer in the Workbench left-pane.
- Double-click Marquee Manager Administrator (in the left or right-pane).
The Marquee Manager Administrator opens.
-
Click New Marquee Server on the Marquee Manager Administrator toolbar.
A Select Data Source dialog box opens.
-
Select the Marquee Manager Server data source.
Default MMSERVER -
Click OK.
Server configuration includes the following tabs.
- Details Tab
- Settings Tab
- Security Tab
Details Tab
Select the Details tab; options are as follows.
Field Description Server Host Name TCP/IP resolvable name for the machine running Marquee Manager Server. This will be in your DNS server or local host file and can be reached from the Administrator workstation. Description (Optional) Additional details about the Server. Connection DSN Automatically entered. User Name Optional. Password Optional. Logging Path Log Path required to access the logs directory on the current Marquee Manager Server. In most cases, if the server is locally installed this path will be a drive letter based directory specification Example C:\Program Files(x86)\Proficy\Proficy CIMPLICITY\MARQUEEMANAGER\Logs\ If the server being managed is not the local server then this path will most likely be a UNC path (\\server\share\directory\), which provides access to the remote servers log directory. Example \\LAB1\MMServer\logs\). Settings Tab
Select the Settings tab.
If the Server: The Settings contain: Has never been configured Defaults Is already configured and operational Configured specifications Options are as follows.
Field Description Server Server Port Port that connects to the Marquee Manager Server. Defaults to 8011. License Key Valid Marquee Manager license key. Delay/Timeout Clock Sync Automatically syncs the internal marquee times to that of the Marquee server. Important: It is recommended that you run NTP (Network Time Protocol) on the Marquee Server machine to set the clock. This will ensure the accuracy of all marquee internal times. Default is 3600 seconds (1 hour). Logging Log Days Number of days the log file will be kept before being purged. Default is 7 days. Log Level For use at the request of the Marquee Manager. In the event of any problems, CIMPLICITY may request additional levels of logging to assist in problem solving. Default is 0. Maximum Space Amount of space to allot to the log file. Note: This prevents the log files from consuming too much drive space. Default is 50 MB. Path Path specification, local to the actual Marquee Manager Server. Note: The path contains the directory where the Marquee Manager Server will store its log files. Click Save.
Important: If you are setting up Remote Administrator, the Settings Tab will already be populated.Security Tab
If security is enabled a Login dialog box will open when a user tries to open the Marquee Manager Administrator window. Only users who have been configured in the Marquee Manager Administrator Tools: Users tree will have access.
Select the Security tab: security options for the selected server are as follows.
Field Description Security Mode Security options for the Marquee Manager server are as follows. NONE Marquee Manager security is not enabled for the server. Windows A valid user name/password are required. Security is as follows. - A Users folder is added to the Tools tree.
- Users who should have access to the Marquee Manager server need to be added.
- A Login dialog box opens when a user attempts to open the Alarm Administrator window.
Windows Trusted Uses a trusted domain account; does not require a password. - A Users folder is added to the Tools tree.
- Users who should have access to the Marquee Manager server need to be added.
Default NONE Important: If you change the Security mode for Windows/Windows Trusted after you have registered users, the users will be deleted. You will have to add users who can be registered for the newly selected mode. - A Users folder is added to the Tools tree.
- Users who should have access to the Marquee Manager server need to be added.
-
A Login dialog box opens when a user attempts to open the Alarm Administrator window.
- A Users folder is added to the Tools tree.
- Users who should have access to the Marquee Manager server need to be added.