System Sentry Devices Screen
About this task
The Devices screen provides statistics concerning the communication to a factory device.
todo: To choose a device for evaluation:
Procedure
-
Click the button to the right of the Device ID bar.
The Select a Device dialog box opens.
-
Select the device to be evaluated.
guide: Guidelines for reading the Devices screen include:
- Review the number of transmissions per second (Transm/Sec) and responses per second (Resp/Sec) to and from the device are meeting your polling requirements.
- Make sure Failures and Retries are zero. Non-zero values indicate a problem. They could indicate that the device is being turned off or the communication link to the device is periodically failing.
- Check the Skipped Polls to determine if too many points are being polled too fast. If they are, you will need to reduce the polling rate to a rate that can be sustained by the communication media and PLC.