About Classes and Class Objects
Instead of repeating the same configuration for components that have similar requirements, you can create the basic configuration for those components as a template to use as a configuration starting point for each.
The CIMPLICITY tools that provide this capability are Classes and Objects.
Item | Description |
---|---|
Classes | A Class is a template that:
A class can be exported in a single .soc file. A custom help file can be created with third party tools and also associated with the class. Beginning in CIMPLICITY 9.5, there are Composite Classes and Objects. Classes can reference other classes. You can modify a class dynamically and you can also delete a class dynamically if there are no references to the class or no object instances of that class with composite references to the class. Read more about Composite Classes here. |
Objects | As many objects as needed can be created based on a single class template. An Object is one instance that is created using a class as a template. An object can be whatever you define it to be. Object configuration takes advantage of the work that went into creating the class. This can greatly reduce repetition that would otherwise be required if configuration for each object was done independently. If a value that was entered as a default value for a class is changed for a selected object in that class, the object's value will not be overwritten if the default class value is changed. |