About Process Health Parameters
Process Health Parameters enables you to have any selected CIMPLICITY project process automatically monitored.
Warning: Keep in mind, restarting a process can have serious consequences, for example losing point values or disconnecting users who are logged in from other locations.
If selected, monitoring can include attempted process restarts, process failure and/or project failure.
Step 1 | Open the Process Health dialog box. |
Step 2 | Enter Process Monitor specifications. |
Note: If Configuration Securityis enabled, only roles that have Projectschecked on the Configuration tab in the Roles dialog box will have access to the Process Health parameters configuration.
Note: The Event Manager Resident Process (EM_RP) reports bad health when it encounters
scenarios where string and/or stack space has been used up or overrun. You can use the
Process Health Parameters application to choose appropriate actions for this
scenario.