About the OEM Key
About this task
OEM Key: Use
The OEM Key:
- Is used for systems that do not have development servers and, more often than not, do not have development viewers.
- Enables OEMs to:
Procedure
- Remotely connect to a CIMPLICITY system or get directly onto the system.
-
Perform whatever configuration changes are needed.
OEM KEY: Limitations
The OEM Key:
- Automatically ends development mode on the runtime server in two hours.
- Requires stopping any running projects twice.
Any projects that are running must be stopped:
- Before the OEM Key can be activated.
-
When the OEM Key terminates (automatically or if it is exited before the two hours).
Note: Projects are stopped automatically when the OEM Key terminates or is exited.
- Makes the runtime server a stand-alone machine; it cannot communicate at all with its viewers while the OEM Key is active.