Syntax
|
CVErr
(expression)
|
Description
|
Converts expression to an error.
|
Comments
|
This function is used to convert an expression into a user-defined error number.
A runtime error is generated under the following conditions:
If expression is
Null
.
If expression is a number outside the legal range for errors, which is as follows:
0 <= expression <= 65535
If expression is
Boolean
.
If expression is a
String
that can't be converted to a number within the legal range.
Empty
is treated as 0.
|
Example
|
This example simulates a user-defined error and displays the error number.
Sub Main()
MsgBox "The error is: " & CStr(CVErr(2046))
End Sub
|
See Also
|
CCur (function); CBool (function); CDate, CVDate (functions); CDbl (function); CInt (function); CLng (function); CSng (function); CStr (function); CVar (function), IsError (function).
|