Syntax
|
GetSetting([ appname], section, key[ , default])
|
Description
|
Retrieves an specific setting from the system registry.
|
Comments
|
The GetSetting function has the following named parameters:
|
|
Parameter
|
Description
|
|
appname
|
String expression specifying the name of the application from which the setting will be read.
|
|
section
|
String expression specifying the name of the section within appname to be read.
|
|
key
|
String expression specifying the name of the key within section to be read.
|
|
default
|
An optional String expression specifying the default value to be returned if the desired key does not exist in the system registry. If omitted, then an empty string is returned if the key doesn’t exist.
|
Example
|
Sub Main()
SaveSetting appname := "NewApp", section := "Startup", _
key := "Height", setting := 200
SaveSetting appname := "NewApp", section := "Startup", _
key := "Width", setting := 320
MsgBox GetSetting(appname := "NewApp", section := "Startup", _
key := "Height", default := "50")
DeleteSetting "NewApp" ' Delete the NewApp key
End Sub
|
See Also
|
GetAllSettings (function), DeleteSetting (statement), SaveSetting (statement)
|
Note
|
Under Win32, this statement operates on the system registry. All settings are read from the following entry in the system registry:
HKEY_CURRENT_USER\Software\BasicScript Program Settings\appname\section\key
On this platform, the appname parameter is not optional.
|