Point Alarm Acknowledge Actions
A Point Alarm Acknowledge action acknowledges the alarm defined by the Alarm ID and Resource ID.
To create this Action, enter the following information in the New Action dialog box:

1 | Alarm ID |
2 | Resource |
1 | Alarm ID |
ID of an alarm to be acknowledged.
(Optional) Click either of the following to select the alarm ID.
![]() |
Browse button | Opens the Alarm browser. |
![]() |
Popup Menu button | Displays Popup menu to create a new alarm, browse for or edit an existing alarm |
2 | Resource |
Resource of the alarm to be acknowledged.
Note: This field is automatically filled in, when an Alarm ID is entered, with the resource assigned to the alarm.
(Optional) Click either of the following to select the alarm ID.
![]() |
Browse button | Opens the Resource browser. |
![]() |
Popup Menu button | Displays Popup menu to create a new resource, browse for or edit an existing resource. |