Syntax
|
Right[$] (string, length)
RightB[$] (string, length)
|
Description
|
Functions return the rightmost length for the following.
|
|
Function
|
Returns rightmost length for;
|
|
Right and RightB
|
Characters
|
|
RightB and RightB$
|
Bytes
|
Comments
|
Functions return the following.
|
|
Functions
|
Return
|
|
Right and RightB
|
String variant
|
|
Right$ and RightB$
|
String
|
|
These functions take the following named parameters:
|
|
Parameter
|
Description
|
|
string
|
String from which characters are returned. A runtime error is generated if string is NULL.
|
|
length
|
Integer specifying the number of characters or bytes to return as follows.
|
|
|
Length is
|
Returns
|
|
|
0
|
Zero-length string is returned.
|
|
|
Greater than or equal to the length of the string
|
String is returned.
|
|
|
The RightB and RightB$ functions are used to return byte data from strings containing byte data.
|
Example
|
'This example shows the Right$ function used in a routine to
'change uppercase names to lowercase with an uppercase first
'letter.
Sub Main()
lname$ = "WILLIAMS"
x = Len(lname$)
rest$ = Right$(lname$,x - 1)
fl$ = Left$(lname$,1)
lname$ = fl$ & LCase$(rest$)
MsgBox "The converted name is: " & lname$
End Sub
|
See Also
|
Left, Left$, LeftB, LeftB$ (functions)
|