Syntax
|
StrComp
(string1,string2 [,compare])
|
Description
|
Returns an
Integer
indicating the result of comparing the two string arguments.
|
Comments
|
Any of the following values are returned:
|
|
0
|
string1
=
string2
|
|
1
|
string1
>
string2
|
|
-1 |
string1
<
string2
|
|
NULL
|
string1 or string2 is
Null
|
|
|
The StrComp function accepts the following parameters:
|
|
Parameter
|
Description
|
|
string1
|
First string to be compared, which can be any expression convertible to a String.
|
|
string2
|
Second string to be compared, which can be any expression convertible to a String.
|
|
compare
|
Optional Integer specifying how the comparison is to be performed. It can be either of the following values:
|
|
|
|
0
|
Case-sensitive comparison
|
|
|
|
1
|
Case-insensitive comparison
|
|
If compare is not specified, then the current
Option Compare
setting is used. If no
Option Compare
statement has been encountered, then
Binary
is used (that is, string comparison is case-sensitive).
|
Example
|
This example compares two strings and displays the results. It illustrates that the function compares two strings to the length of the shorter string in determining equivalency.
Const crlf = Chr$(13) + Chr$(10)
Sub Main()
Dim abc As Integer
Dim abi As Integer
Dim cdc As Integer
Dim cdi As Integer
a$ = "This string is UPPERCASE and lowercase"
b$ = "This string is uppercase and lowercase"
c$ = "This string"
d$ = "This string is uppercase and lowercase characters"
msg1 = "a = " & a & crlf
msg1 = msg1 & "b = " & b & crlf
msg1 = msg1 & "c = " & c & crlf
msg1 = msg1 & "d = " & d & crlf & crlf
abc = StrComp(a$,b$,1)
msg1 = msg1 & "a and c (insensitive) : " & abc & crlf
abi = StrComp(a$,b$,0)
msg1 = msg1 & "a and c (sensitive): " & abi & crlf
cdc = StrComp(c$,d$,1)
msg1 = msg1 & "c and d (insensitive): " & cdc & crlf
cdi = StrComp(c$,d$,0)
msg1 = msg1 & "c and d (sensitive) : " & cdi & crlf
MsgBox msg1
End Sub
|
See Also
|
Comparison Operators (topic); Like (operator); Option Compare (statement).
|
|
|
|
|
|