Transition Set Actions
A Transition Set action sets the value of the point in the Point ID to the value of the point in the Point ID field of the Event associated with this Action.
To create this Action, enter the following information in the New Action dialog box

Point ID |
ID of a point that will be updated with the value of an associated event's point ID. Valid entries are either a device or global point ID
(Optional) Click either of the following to select the alarm ID.
![]() |
Browse button | Opens the Point browser. |
![]() |
Popup Menu button | Displays Popup menu to create a new point, browse for or edit an existing point. |