Resume Scripts
Procedure
- Select the actions whose scripts you want to resume in the BCEUI window. You can use the Shift and Ctrl keys to select multiple actions.
-
Do one of the following.
- Select Resume from the Scripts menu, or
- Click the Resume Scripts button on the toolbar, or
- Select Resume from the Window Pop-up menu.
The Confirm Resume dialog box opens.
-
You may select one of the following.
Yes to All Resume all the selected scripts. Yes Resume this script. No Cancel the resume request for this script. Cancel Cancel your request. Note: If you click Yes or No and you are resuming multiple scripts, you are automatically prompted to confirm the next script in the list.