Stop Scripts
Procedure
- Select the actions whose scripts you want to stop in the BCEUI window. You can use the Shift and Ctrl keys to select multiple actions.
-
Do one of the following.
- Select Stop from the Scripts menu, or
- Click the Stop Scripts button on the toolbar, or
- Select Stop from the Window Pop-up Menu.
The Confirm Stop dialog box opens.
-
Click one of the following.
Yes to All Stop all the selected scripts. Yes Stop this script. No Cancel the stop request for this script. Cancel Cancel your request. Note: If you click Yes or No and you are stopping multiple scripts, you are automatically prompted to confirm the next script in the list.
Results
The status of the scripts for the events you select changes from Paused or Running to Stopped and the message field for each stopped script displays the line number where the script was stopped.
Note: Once you stop a script, you cannot restart it with the Resume command.