Conveyance System IDs
The Conveyance System ID is a string of up to four characters, which is appended to label values for certain label formats. Each label reader has a Conveyance System ID associated with it.
The device communication enabler initializes Conveyance System IDs to an empty string when it starts up and accepts setpoint requests to assign them at run time.
One mechanism for these setpoints is to use the Basic Control Engine, create events to check for the IDs being blank, and associated actions to set them to the desired value. In this way, each time the enabler restarts, the desired Conveyance System IDs are initialized.